Configuration
Configure the email behavior that are being sent from your account in the Configuration section.
Configuration screen
Perform the following configurations to define the email behavior:
-
Turn the Send Email toggle off for not sending any emails from the configured accounts.
-
Turn the Send email to test email id toggle on to send the test mails to the test server. You can also define the test email ID to receive the test emails.
-
Define the maximum attachment size that can be added to an email in Email attachment max size option.
-
Provision the SMTP error code to resend the emails if the selected error occurs. To do that, select the SMTP error codes in the Retry email if the server returns these SMTP error codes dropdown.
-
Define the maximum number of times the email can be resent in Number of retries option.
-
Define the interval in which the email can be resent in the Retry interval (in minutes) option.
Click Save to update the configuration settings for the configured accounts.